AIN#.OFFSET
Description
AIN#.OFFSET sets the analog offset, which is added to the analog input command to the drive. This value compensates for the analog input signal (AIN#.VALUE) offset or drift.
-
- AIN#.ZERO will set this value.
Examples
Code
--> AIN1.VALUE 0.056 V --> AIN1.OFFSET -0.056 --> AIN1.VALUE 0.000 V
Context
For more information see Analog Input.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | V |
| Range | -10V to +10V |
| Default Value | 0 V |
| Data Type | Float |
| See Also | |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.